GLONASS Almanac – AGL format

File Name format: ???_< YYYY> <MM> <DD> <HH>. Agl

 

Here is an example: STN_2010011022.Agl

1) The almanac is an ascii (8 bit characters) text file with lines separated by <CR> or <CR><LF>

2) The Almanac is a series of “entries”

3) Each “entry” represents almanac data for one space vehicle or satellite in the Glonass constellation at a particular time/date.

4) Each “entry” is three lines of the file and has 20 numbers plus an optional comment which could be non-numeric

5) Each line of an “entry” is some numeric values with one or more spaces between values, the first line could optionally have a comment at the end which could be non-numeric

6) Integers may have leading zeros “01” .vs. “1”

7) Non integers are in “E” format: “0.273825937E+05 “ is the number 27382.5937

8) There are no blank lines between “entries”, there are no optional comment lines

9) The file starts with line 1 of the first entry

10) There can be a large number of “entries” in an AGL file with almanac data valid at different times and for different satellites (space vehicles)

 

Here is an example of an “entry” – there are three lines of the text file.

01 01 2011 1800 COMMENT

1 1 1 01 01 2011 0.273825937E+05 0.000000000E+00 0.000000000E+00 0.179290771E-03

0.5286379E+00 0.9077072E-02 -0.1849365E-01 0.5264282E-03 -0.2655781E+04 -0.1586914E-02

 

Here are the descriptions of the data on the three lines. Data is separated by one or more spaces.

Line 1

1 – day of Almanac

2 - month of Almanac

3 - year of Almanac

4 - time of receipt of the Almanac from the beginning of the day, UTC

5 – optional comment (with which the receiver is received, SW version etc.)

Line 2

1 - number of spacecraft in the grouping (orbital slot number)

2 - number of frequency channel (-7 .. 6)

3 – SV health indicator (0 -> bad, 1 -> healthy, operational)

4 - day

5 - month

6 - year

7 - the reference time of the almanac

8 – Correction from GLONASS to UTC

9 – Correction to GPS time relative GLONASS

10 - Correction of time relative to GLONASS system time,

Line 3

1 – Lamda - longitude of first ascending node passage, angle in semi-cycles

2 - dI - correction to the mean value of inclination, in semi-cycles

3 - w - argument of perigee, in semi-cycles

4 - E - eccentricity

5 - dT - correction to the mean value of Draconian period, in second

6 - dTT - rate of change of Draconian period, in second / coil